Other Parts Discussed in Thread: LM5026
求助 TI技术人员大家好,求助
问题一:在UCC2897A的应用文件SLUA535中的第12页的第9式中,
问题二:请问,在UCC2897A的应用文件SLUA535中的第17页的第23式中,是否少乘了Iqf(RMS)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求助 TI技术人员大家好,求助
问题一:在UCC2897A的应用文件SLUA535中的第12页的第9式中,
问题二:请问,在UCC2897A的应用文件SLUA535中的第17页的第23式中,是否少乘了Iqf(RMS)?
Hello Dushimutong
My TI translator app gives me the following translation and I'll answer as best I can - in red
Problem: In UCC2897A SLUA 535 of shop 9 on Page 12 of the application file(s)
The values given by Calculation formulas are not would be 285.568 does uF, is an error for an error or formula?
I think that the formula is correct, but the values of the parameters that go into it are not very clear. You need to know the gate charge of the MOSFETs you are driving and the switching frequency. You also need to know the capacitance at the VREF pin - I assumed 0.22uF. The equation is dominated by the charge needed to switch the MOSFET gates and by the soft start time. None of this is particularly clear in the app note - so my advice would be to use the equation as is and to see what sort of start-up time you can get with a 330uF capacitor. For example, if you set tss to 200ms, and Ic = 3mA and Qg = 30nC and Vhyst = 4.4V you will get a Cboot of 3007uF.
Issue 2: Does in UCC2897A SLUA 535 of the section on Page 17 of the application file(s) 23, is it less by the Iqf (RMS) ?
I'm not sure I understand your question but Equation 23 calculates only the switching loss of QF. the forward conduction losses in the Rds_on will add to this loss (calculated in equation 26) as will the conduction losses if the body diode conducts for some of the switching cycle, (calculated in equation 25)
Question 3: In UCC2897A SLUA 535 of page 54on Page 25 of the application file(s)
1: Qgc definition of what is?
I think you mean Equation 54 on Page 25 - Qgc is the gate charge of the MOSFET - this is usually given in the MOSFET datasheet. Equation 54 is calculating an effective capacitance from gate to drain. It has been extrapolated from the MOSFET datasheet. This effective capacitance is then used to estimate the switching losses in the main MOSFET (equation 55)
2: Qmain is main MOS tube DP of Si7846 is the total gate charge Qg?
I'm sorry but I don't understand this question.
Question 4: In UCC2897A SLUA of the application file(s) 535, gain/frequency curves is MathCAD Calculation or Simulation of the idea of which software I can I use as a formula simulation diagram thank follow some difference between figure on the material. TI never released a MathCAD file for this device but there is an internal file that you may find helpful - attached.
/cfs-file/__key/communityserver-discussions-components-files/196/2768.UCC2897A_5F00_Power-Stage-Design_5F00_Rev-0.xmcd
Please let me know if I can be of any further help.
Regards
Colin
Helo Colin
Thank you very much.
问题2中:公式23中,开关损耗的计算时,如果不引入电流,则公式得不到功率单位瓦特(W)。
问题3中:公式54中,如果Qgc代表MOS的栅极电荷,那Qmain代表什么呢。也就是说,我不知道引入什么数据来计算。
问题4中:这个SLUA535文件,中的Figure20,Figure21,Figure22,Figure23,Figure24,Figure25,Figure26,Figure27,是用什么软件仿真的?
Regards
dushimutong
Hello Dushimutong
: formula of 23 in the calculation of switching losses, if does not introduce a current, the formula would lose Solutions power in watts (W) in question 2.
I'm sorry, Equation 23 is dimensionally incorrect - it calculates a Voltage (V) and you are correct - this needs to be multiplied by a Current (A) to give a Power (W). Assuming that the current is 33nC*250kHz then I calculate as follows 5V*16.5ns*250kHz*33nC*250kHz = 0.17mW This is in line with my expectation that the switching losses on the low voltage output are very small - I think the 506mW in the app note is an overestimate.
Question 3: In equation 54 is calculated if MOS Qgc represents what about gate charge - the Qmain representative. That is, I'm not sure what data is introduced.
COSS_QMAIN_100V is taken from the MOSFET datasheet - it is the Coss value at a drain to source voltage of 100V. The COSS_QAUX_100V is the same parameter for the Aux MOSFET.
SLUA for question 4: This 535 files in Figure 20, Figure 21, Figure 22, Figure 23, Figure 24, Figure 25, Figure 26, Figure 27 that is to use what software emulation? It's not possible to say - the original graphs may have been generated in MathCAD or possibly in EXCEL. The Technical Writer would normally take these source files and re-format them into a standard TI format -
My TI translator isn't doing a very good job but I think you are asking about where you can download the Unitrode SEM-1100 paper - This may be found at http://www.ti.com/ww/en/power-training/login.shtml?DCMP=psdslibrary&HQS=tlead-power-psdslibrary-apec2015-pwrhouse-20150312-lp-en - along with all the other design seminar papers - It's organised along topic lines not by seminar number but if you put 'sem-1100' into the search field you may find the topic you need.
Please let me know if you need any further help.
Regards
Colin
Hello Dushimutong
No - I'm sorry we don't have an Mathcad file for the LM5026.
You may find the information in the .pdf at www.ti.com/.../slua672.pdf useful.
You probably have already found the SEM1000 material but the SEM1000 topics at https://www.ti.com/seclit/ml/slup108/slup108.pdf and https://www.ti.com/seclit/ml/slup112/slup112.pdf may be of help.
Regards
Colin