This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23754: TPS23754 protection mechanism

Part Number: TPS23754

Dear Sir,

I am studying TPS23754 POE-PD solution and will use TPS23754EVM-383 as our prototype board.  But  may I know the TPS23754 protection mechanism? when  over current occur, how is the behavior of TPS23754? will it hiccup or shutdown?

Since we need to send a signal to MCU while TPS23754 failure occur. How do we get this signal? or should we add external circuit? Thanks.

  • Hi Lucifer,

    Typically, the converter's current limit will be the first line of defense for a fault on the output load. In this case, the converter will hiccup. Next will be the PSE's current limit in which the PSE will foldback or shutdown. Lastly, depending how fast the fault is, the PD as a current limit in which the VDD/RTN voltage will foldback or go into inrush as shown in it's datasheet.

    Since there is multiple points of the protection, it'll be difficult to choose any particular one to feed a signal to flag a fault. Is the MCU on the load side? How will it process a fault if for example there is short on the output and there is no regulated power on the MCU?
  • Hi Darwin,
    The MCU i s a core chip of the platform. it will collect all system information for user. therefore we need a indicated signal to show the TPS23754 working status. Thanks.