I'm trying to drive a LED string of 12 HB LEDs at a maximum current of 100mA
Supply voltage is 5V.
LED forward voltage is: 3.1V
Can TPS61169 support this application?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to drive a LED string of 12 HB LEDs at a maximum current of 100mA
Supply voltage is 5V.
LED forward voltage is: 3.1V
Can TPS61169 support this application?
Hi Randy,
Thanks for pointing that out to me.
I have another LED string in my design with 4 NIR LEDs, each has maximum forward voltage of 3.5V.
I build a driver using TPS61169 with L=10uH, Cout=10uF and Rset=2 ohms but couldn't get the driver to output enough current/voltage to drive the LED string with 100mA.
Is there a limit to the maximum power I can get out of this device?
Thanks,
Udi
Hi Randy,
Both current and voltage measured below what I would expect.
Is there a way I can send you drawings of the board layout?
Best regards,
Udi