This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3: Simultaneous temperature and SOC charge inhibition possible?

Part Number: BQ27510-G3

Hey everyone,

In our design, we use a BQ27510-G3 in conjunction with a BQ24040 charger IC, they are connected via GPOUT -> TS. I've configured the gas gauge to inhibit charging when the battery reaches certain temperature thresholds (by setting PFC_CFG to 01 inside OpConfig). I was wondering if it is possible with this setup to incorporate a simultaneous logic to enable/disable charging according to the battery's state of charge as well (f.i. below x % soc, don't let the charging begin). We would consider to add this in order to enhance the battery's lifetime. Would this work side by side and if yes, which configuration parameters need to be changed?

Thanks!