This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27211A: Output current

Part Number: UCC27211A


Hi

I have some question for this device.

- How dose this device limit the output current?

- Can this device output over 4A if it is short time?

  ( Does this device clamp the output current if the output current exceed 4A?)

Regards,

Koji Hamamoto

  • Hamamoto-san,

    Thank you for your interest in the UCC27211A gate driver.  The output current is governed by the output stage rDSON -- there is no active current limiting circuit. The typical peak (i.e.,max) output current is 4A. Since, as mentioned above, there is no limiting or clamping circuit, the current could be a little higher or lower than 4A based on part to part variations, but I do not recommend designing under the assumption of more than 4A max/peak current.

    Regards,

    - Daniel