This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z60: BQ40z60

Part Number: BQ40Z60

I am using the bq40z60 part.  I have completed the following:  Downloaded the correct cell chemistry file, edited the gg.csv file with the appropriate information, performed calibration, and performed the optimization cycles for this battery pack.  The Qmax has been updated to 0E and the Ra tables have been updated.

I read an earlier post that states the following

 

Here are the steps to create the golden srec file.

•Run the Optimization Cycle to update Qmax and the Ra-table.

•Go to the Data Flash window and press the Read All button.

•Export the gg.csv file

•Edit the gg.csv file using a text editor. e.g. Notepad. Do not use Excel.

•Set the Update Status to 02 and set the Cycle Count to 0.

•Load the default .srec file into the device.

•Load the ChemID into the device.

•Load your modified gg.csv file into the device and press the Write All button. (Be sure to import the calibration data as well.)

•Save the golden .srec file.

 

Question  -- Since I have completed these steps already shouldn't I just have to change the Update Status to 02 and the cycle count to 0 in BQ Studio and save the .srec file as the Golden Image?  If not could you please explain the reason?

 

Thanks

 

Cliff

  • You may be able to edit the DF directly and change these parameters. There are a few reasons that we recommend the other procedure.

    • Some devices do not have both Cycle Count parameters available in DF, so you would not be able to change them directly. 
    • There are hidden areas of DF that get cleared when you load the default srec and these do not get cleared if you just change these parameters directly.
    • We try not to deviate from the general procedure, because this confuses people.

  • Thanks Tom

    Could you send me a link to the BQ40z60 default gg.csv ?
  • We do not have a default gg.csv file published. You can download the default srec file from the bq40z60 product website and it is located under Software.
  • Tom
    I am having trouble making the golden image. I downloaded the default .srec file and then the chemistry file followed by the updated gg.csv file. I noticed that the update status and the cycle count were correct but when I hit Write All the data memory displayed default data. Did I miss something ?
  • That process is correct. Send your gg file and which ChemID you are using and I will create the golden srec for you.
  • OK Tom The Chem ID is 2012 and here is the gg.csv.
    * Texas Instruments Data Flash File
    * File created Wed Feb 15 15:30:52 2017
    *
    * Device Number 4600
    * Firmware Version 0.15
    * Build Number 21
    * Order Number 0
    *
    * bqz Device Number 4600
    * bqz Firmware Version 0.15
    * bqz Build Number 21
    *
    * Field Order: Class name Subclass name Parameter name Parameter Value Display Units
    Calibration Voltage Cell Gain 12131 -
    Calibration Voltage Pack Gain 50157 -
    Calibration Voltage BAT Gain 49182 -
    Calibration Current CC Gain 4.983 mOhm
    Calibration Current Capacity Gain 4.982 mOhm
    Calibration Current Offset CC Offset 0 -
    Calibration Current Offset Coulomb Counter Offset Samples 64 -
    Calibration Current Offset Board Offset 0 -
    Calibration Current Offset CC Auto Config 7 hex
    Calibration Current Offset CC Auto Offset -3 -
    Calibration Temperature Internal Temp Offset 0.7 degC
    Calibration Temperature External1 Temp Offset -0.1 degC
    Calibration Temperature External2 Temp Offset -0.4 degC
    Calibration Temperature External3 Temp Offset -1.1 degC
    Calibration Temperature External4 Temp Offset -1 degC
    Calibration Internal Temp Model Int Gain -12143 -
    Calibration Internal Temp Model Int base offset 6232 -
    Calibration Internal Temp Model Int Minimum AD 0 -
    Calibration Internal Temp Model Int Maximum Temp 6232 0.1degK
    Calibration Cell Temperature Model Coeff a1 -11130 -
    Calibration Cell Temperature Model Coeff a2 19142 -
    Calibration Cell Temperature Model Coeff a3 -19262 -
    Calibration Cell Temperature Model Coeff a4 28203 -
    Calibration Cell Temperature Model Coeff a5 892 -
    Calibration Cell Temperature Model Coeff b1 328 -
    Calibration Cell Temperature Model Coeff b2 -605 -
    Calibration Cell Temperature Model Coeff b3 -2443 -
    Calibration Cell Temperature Model Coeff b4 4696 -
    Calibration Cell Temperature Model Rc0 11703 -
    Calibration Cell Temperature Model Adc0 11703 -
    Calibration Cell Temperature Model Rpad 0 -
    Calibration Cell Temperature Model Rint 0 -
    Calibration Fet Temperature Model Coeff a1 -11130 -
    Calibration Fet Temperature Model Coeff a2 19142 -
    Calibration Fet Temperature Model Coeff a3 -19262 -
    Calibration Fet Temperature Model Coeff a4 28203 -
    Calibration Fet Temperature Model Coeff a5 892 -
    Calibration Fet Temperature Model Coeff b1 328 -
    Calibration Fet Temperature Model Coeff b2 -605 -
    Calibration Fet Temperature Model Coeff b3 -2443 -
    Calibration Fet Temperature Model Coeff b4 4696 -
    Calibration Fet Temperature Model Rc0 11703 -
    Calibration Fet Temperature Model Adc0 11703 -
    Calibration Fet Temperature Model Rpad 0 -
    Calibration Fet Temperature Model Rint 0 -
    Calibration Current Deadband Deadband 3 mA
    Calibration Current Deadband Coulomb Counter Deadband 9 116nV
    Settings Protection Protection Configuration 0 hex
    Settings Protection Enabled Protections A ff hex
    Settings Protection Enabled Protections B 7f hex
    Settings Protection Enabled Protections C d5 hex
    Settings Protection Enabled Protections D 2f hex
    Settings Permanent Failure Enabled PF A 0 hex
    Settings Permanent Failure Enabled PF B 0 hex
    Settings Permanent Failure Enabled PF C 0 hex
    Settings Permanent Failure Enabled PF D 0 hex
    Settings Configuration Charging Configuration 0 hex
    Settings Configuration Temperature Enable 1f hex
    Settings Configuration Temperature Mode 1 hex
    Settings Configuration DA Configuration 13 hex
    Settings Configuration FET Options 20 hex
    Settings Configuration Sbs Gauging Configuration 4 hex
    Settings Configuration Sbs Configuration 21 hex
    Settings Configuration Power Config 0 hex
    Settings Configuration IO Config 0 hex
    Settings Configuration LED Configuration 0 hex
    Settings Configuration SOC Flag Config A 0c8c hex
    Settings Configuration SOC Flag Config B 8c hex
    Settings Configuration Balancing Configuration 7 hex
    Settings Configuration IT Gauging Configuration d4fe hex
    Settings AFE AFE Protection Control 70 hex
    Settings AFE ZVCHG Exit Threshold 2200 mV
    Settings Fuse PF Fuse A 0 hex
    Settings Fuse PF Fuse B 0 hex
    Settings Fuse PF Fuse C 0 hex
    Settings Fuse PF Fuse D 0 hex
    Settings Fuse Min Blow Fuse Voltage 3500 mV
    Settings Fuse Fuse Blow Timeout 30 s
    Settings BTP Init Discharge Set 150 mAH
    Settings BTP Init Charge Set 175 mAH
    Settings Manufacturing Mfg Status init 618 hex
    Protections CUV Threshold 2500 mV
    Protections CUV Delay 2 s
    Protections CUV Recovery 3000 mV
    Protections CUVC Threshold 2400 mV
    Protections CUVC Delay 2 s
    Protections CUVC Recovery 3000 mV
    Protections COV Threshold Low Temp 4300 mV
    Protections COV Threshold Standard Temp 4300 mV
    Protections COV Threshold High Temp 4300 mV
    Protections COV Threshold Rec Temp 4300 mV
    Protections COV Delay 2 s
    Protections COV Recovery Low Temp 3900 mV
    Protections COV Recovery Standard Temp 3900 mV
    Protections COV Recovery High Temp 3900 mV
    Protections COV Recovery Rec Temp 3900 mV
    Protections ACOV Threshold 20000 mV
    Protections ACOV Recovery 19000 mV
    Protections OCC1 Threshold 6000 mA
    Protections OCC1 Delay 6 s
    Protections OCC2 Threshold 8000 mA
    Protections OCC2 Delay 3 s
    Protections OCC Recovery Threshold -200 mA
    Protections OCC Recovery Delay 5 s
    Protections OCD1 Threshold -6000 mA
    Protections OCD1 Delay 6 s
    Protections OCD2 Threshold -8000 mA
    Protections OCD2 Delay 3 s
    Protections OCD Recovery Threshold 200 mA
    Protections OCD Recovery Delay 5 s
    Protections AOLD Latch Limit 0 -
    Protections AOLD Counter Dec Delay 10 s
    Protections AOLD Recovery 5 s
    Protections AOLD Reset 15 s
    Protections AOLD Threshold f4 hex
    Protections ASCC Latch Limit 0 -
    Protections ASCC Counter Dec Delay 10 s
    Protections ASCC Recovery 5 s
    Protections ASCC Reset 15 s
    Protections ASCC Threshold 77 hex
    Protections ASCD Latch Limit 0 -
    Protections ASCD Counter Dec Delay 10 s
    Protections ASCD Recovery 5 s
    Protections ASCD Reset 15 s
    Protections ASCD Threshold 1 77 hex
    Protections ASCD Threshold 2 e7 hex
    Protections OTC Threshold 55 1degC
    Protections OTC Delay 2 s
    Protections OTC Recovery 50 1degC
    Protections OTD Threshold 85 1degC
    Protections OTD Delay 45 s
    Protections OTD Recovery 55 1degC
    Protections OTF Threshold 85 1degC
    Protections OTF Delay 2 s
    Protections OTF Recovery 65 1degC
    Protections UTC Threshold 5 1degC
    Protections UTC Delay 2 s
    Protections UTC Recovery 8 1degC
    Protections UTD Threshold 0 1degC
    Protections UTD Delay 2 s
    Protections UTD Recovery 5 1degC
    Protections COT Recovery Delay 5 s
    Protections HWD Delay 10 s
    Protections PTO Charge Threshold 2000 mA
    Protections PTO Suspend Threshold 1800 mA
    Protections PTO Delay 1800 s
    Protections PTO Reset 2 mAh
    Protections CTO Charge Threshold 2500 mA
    Protections CTO Suspend Threshold 2000 mA
    Protections CTO Delay 54000 s
    Protections CTO Reset 2 mAh
    Protections OC Threshold 300 mAh
    Protections OC Recovery 2 mAh
    Protections OC RSOC Recovery 90 %
    Protections CHGV Threshold 500 mV
    Protections CHGV Delay 30 s
    Protections CHGV Recovery -500 mV
    Protections CHGC Threshold 500 mA
    Protections CHGC Delay 8 s
    Protections CHGC Recovery Threshold 100 mA
    Protections CHGC Recovery Delay 2 s
    Protections PCHGC Threshold 50 mA
    Protections PCHGC Delay 2 s
    Protections PCHGC Recovery Threshold 10 mA
    Protections PCHGC Recovery Delay 2 s
    Permanent Fail SUV Threshold 2200 mV
    Permanent Fail SUV Delay 5 s
    Permanent Fail SOV Threshold 4500 mV
    Permanent Fail SOV Delay 5 s
    Permanent Fail SOCC Threshold 10000 mA
    Permanent Fail SOCC Delay 5 s
    Permanent Fail SOCD Threshold -10000 mA
    Permanent Fail SOCD Delay 5 s
    Permanent Fail SOT Threshold 65 1degC
    Permanent Fail SOT Delay 5 s
    Permanent Fail SOTF Threshold 100 1degC
    Permanent Fail SOTF Delay 5 s
    Permanent Fail Open Thermistor Threshold -50 1degC
    Permanent Fail Open Thermistor Delay 5 s
    Permanent Fail Open Thermistor Fet Delta 20 1degC
    Permanent Fail Open Thermistor Cell Delta 20 1degC
    Permanent Fail QIM Delta Threshold 15 %
    Permanent Fail QIM Delay 2 updates
    Permanent Fail CB Max Threshold 240 h
    Permanent Fail CB Delta Threshold 40 h
    Permanent Fail CB Delay 2 cycles
    Permanent Fail VIMR Check Voltage 3500 mV
    Permanent Fail VIMR Check Current 10 mA
    Permanent Fail VIMR Delta Threshold 500 mV
    Permanent Fail VIMR Delta Delay 5 s
    Permanent Fail VIMR Duration 100 s
    Permanent Fail VIMA Check Voltage 3700 mV
    Permanent Fail VIMA Check Current 50 mA
    Permanent Fail VIMA Delta Threshold 200 mV
    Permanent Fail VIMA Delay 5 s
    Permanent Fail IMP Delta Threshold 300 %
    Permanent Fail IMP Max Threshold 400 %
    Permanent Fail IMP Ra Update Counts 2 counts
    Permanent Fail CD Threshold 0 mAh
    Permanent Fail CD Delay 2 cycles
    Permanent Fail CFET OFF Threshold 5 mA
    Permanent Fail CFET OFF Delay 5 s
    Permanent Fail DFET OFF Threshold -50 mA
    Permanent Fail DFET OFF Delay 5 s
    Permanent Fail FUSE Threshold 5 mA
    Permanent Fail FUSE Delay 5 s
    Permanent Fail AFER Threshold 100 -
    Permanent Fail AFER Delay Period 2 s
    Permanent Fail AFER Compare Period 5 s
    Permanent Fail AFEC Threshold 100 -
    Permanent Fail AFEC Delay Period 5 s
    Permanent Fail 2LVL Delay 5 s
    Permanent Fail OPNCELL Threshold 5000 mV
    Permanent Fail OPNCELL Delay 5 s
    Advanced Charge Algorithm Charger Minimum Voltage Output 8369 mV
    Advanced Charge Algorithm Charger Voltage Resolution 33 mV
    Advanced Charge Algorithm Charger LCHG Current Resolution 8 mA
    Advanced Charge Algorithm Charger Current Resolution 39 mA
    Advanced Charge Algorithm Charger Max Current Register 255 -
    Advanced Charge Algorithm Charger Vacp Hysteresis 0 mV
    Advanced Charge Algorithm Temperature Ranges T1 Temp 5 degC
    Advanced Charge Algorithm Temperature Ranges T2 Temp 17 degC
    Advanced Charge Algorithm Temperature Ranges T5 Temp 35 degC
    Advanced Charge Algorithm Temperature Ranges T6 Temp 40 degC
    Advanced Charge Algorithm Temperature Ranges T3 Temp 45 degC
    Advanced Charge Algorithm Temperature Ranges T4 Temp 55 degC
    Advanced Charge Algorithm Temperature Ranges Hysteresis Temp 1 degC
    Advanced Charge Algorithm Low Temp Charging Voltage 3952 mV
    Advanced Charge Algorithm Low Temp Charging Current Low 132 mA
    Advanced Charge Algorithm Low Temp Charging Current Med 352 mA
    Advanced Charge Algorithm Low Temp Charging Current High 264 mA
    Advanced Charge Algorithm Standard Temp Charging Voltage 4151 mV
    Advanced Charge Algorithm Standard Temp Charging Current Low 1200 mA
    Advanced Charge Algorithm Standard Temp Charging Current Med 1200 mA
    Advanced Charge Algorithm Standard Temp Charging Current High 1200 mA
    Advanced Charge Algorithm High Temp Charging Voltage 3952 mV
    Advanced Charge Algorithm High Temp Charging Current Low 1200 mA
    Advanced Charge Algorithm High Temp Charging Current Med 1200 mA
    Advanced Charge Algorithm High Temp Charging Current High 1200 mA
    Advanced Charge Algorithm Rec Temp Charging Voltage 4051 mV
    Advanced Charge Algorithm Rec Temp Charging Current Low 1200 mA
    Advanced Charge Algorithm Rec Temp Charging Current Med 1200 mA
    Advanced Charge Algorithm Rec Temp Charging Current High 1200 mA
    Advanced Charge Algorithm Pre-Charging Current 250 mA
    Advanced Charge Algorithm Maintenance Charging Current 44 mA
    Advanced Charge Algorithm Voltage Range Precharge Start Voltage 2500 mV
    Advanced Charge Algorithm Voltage Range Charging Voltage Low 2900 mV
    Advanced Charge Algorithm Voltage Range Charging Voltage Med 3600 mV
    Advanced Charge Algorithm Voltage Range Charging Voltage High 4000 mV
    Advanced Charge Algorithm Voltage Range Charging Voltage Hysteresis 0 mV
    Advanced Charge Algorithm Termination Config Charge Term Taper Current 250 mA
    Advanced Charge Algorithm Termination Config Charge Term Voltage 75 mV
    Advanced Charge Algorithm Charging Rate of Change Current Rate 1 steps
    Advanced Charge Algorithm Charging Rate of Change Voltage Rate 1 steps
    Advanced Charge Algorithm Cell Balancing Config Bal Time/mAh Cell 1 367 s/mAh
    Advanced Charge Algorithm Cell Balancing Config Bal Time/mAh Cell 2-4 514 s/mAh
    Advanced Charge Algorithm Cell Balancing Config Min Start Balance Delta 3 mV
    Advanced Charge Algorithm Cell Balancing Config Relax Balance Interval 18000 s
    Advanced Charge Algorithm Cell Balancing Config Min Rsoc for Balancing 80 %
    Gas Gauging Current Thresholds Dsg Current Threshold 100 mA
    Gas Gauging Current Thresholds Chg Current Threshold 50 mA
    Gas Gauging Current Thresholds Quit Current 10 mA
    Gas Gauging Current Thresholds Dsg Relax Time 1 s
    Gas Gauging Current Thresholds Chg Relax Time 60 s
    Gas Gauging Current Thresholds Dsg Body Diode Protect Threshold 100 mA
    Gas Gauging Current Thresholds Chg Body Diode Threshold 100 mA
    Gas Gauging Design Design Capacity mAh 6700 mAh
    Gas Gauging Design Design Capacity cWh 9648 cWh
    Gas Gauging Design Design Voltage 14400 mV
    Gas Gauging Cycle Cycle Count Percentage 90 %
    Gas Gauging FD Set Voltage Threshold 2500 mV
    Gas Gauging FD Clear Voltage Threshold 2600 mV
    Gas Gauging FD Set % RSOC Threshold 0 %
    Gas Gauging FD Clear % RSOC Threshold 5 %
    Gas Gauging FC Set Voltage Threshold 4200 mV
    Gas Gauging FC Clear Voltage Threshold 4100 mV
    Gas Gauging FC Set % RSOC Threshold 100 %
    Gas Gauging FC Clear % RSOC Threshold 95 %
    Gas Gauging TD Set Voltage Threshold 2700 mV
    Gas Gauging TD Clear Voltage Threshold 2800 mV
    Gas Gauging TD Set % RSOC Threshold 6 %
    Gas Gauging TD Clear % RSOC Treshold 8 %
    Gas Gauging TC Set Voltage Threshold 4200 mV
    Gas Gauging TC Clear Voltage Threshold 4100 mV
    Gas Gauging TC Set % RSOC Threshold 100 %
    Gas Gauging TC Clear % RSOC Threshold 95 %
    Gas Gauging State Cycle Count 0 -
    Gas Gauging State Qmax Cell 1 6613 mAh
    Gas Gauging State Qmax Cell 2 6628 mAh
    Gas Gauging State Qmax Cell 3 6617 mAh
    Gas Gauging State Qmax Cell 4 6610 mAh
    Gas Gauging State Qmax Pack 6610 mAh
    Gas Gauging State Qmax Cycle Count 7 -
    Gas Gauging State Update Status 2 -
    Gas Gauging State Cell 1 Chg Voltage at EoC 4192 mV
    Gas Gauging State Cell 2 Chg Voltage at EoC 4196 mV
    Gas Gauging State Cell 3 Chg Voltage at EoC 4194 mV
    Gas Gauging State Cell 4 Chg Voltage at EoC 4191 mV
    Gas Gauging State Current at EoC 181 mA
    Gas Gauging State Avg I Last Run -1336 mA
    Gas Gauging State Avg P Last Run -1930 cW
    Gas Gauging State Delta Voltage 16 mV
    Gas Gauging State Temp k 1.73 degC/256mW
    Gas Gauging State Temp a 3204 -
    Gas Gauging State Max Avg I Last Run -1338 mA
    Gas Gauging State Max Avg P Last Run -2191 cW
    Gas Gauging IT Cfg Load Select 7 -
    Gas Gauging IT Cfg Load Mode 0 -
    Gas Gauging IT Cfg Design Resistance 47 mOhms
    Gas Gauging IT Cfg User Rate-mA 0 mA
    Gas Gauging IT Cfg User Rate-cW 0 cW
    Gas Gauging IT Cfg Reserve Cap-mAh 0 mAh
    Gas Gauging IT Cfg Reserve Cap-cWh 0 cWh
    Gas Gauging IT Cfg Pack Resistance 30 mOhms
    Gas Gauging IT Cfg System Resistance 0 mOhms
    Gas Gauging IT Cfg Ra Filter 50 %
    Gas Gauging IT Cfg Ra Max Delta 15 %
    Gas Gauging IT Cfg Reference Grid 4 -
    Gas Gauging IT Cfg Resistance Parameter Filter 65142 -
    Gas Gauging IT Cfg Near EDV Ra Param Filter 59220 -
    Gas Gauging IT Cfg Qmax Delta 5 %
    Gas Gauging IT Cfg Qmax Upper Bound 130 %
    Gas Gauging IT Cfg Term Voltage 9000 mV
    Gas Gauging IT Cfg Term V Hold Time 1 s
    Gas Gauging IT Cfg Term Voltage Delta 300 mV
    Gas Gauging IT Cfg Term Min Cell V 2800 mV
    Gas Gauging IT Cfg Voltage Consistency Delta 300 mV
    Gas Gauging IT Cfg Fast Scale Start SOC 10 %
    Gas Gauging Smoothing Smooth Relax Time 1000 s
    Gas Gauging Condition Flag Max Error Limit 100 %
    Gas Gauging Max Error Time Cycle Equivalent 24 h
    Gas Gauging Max Error Cycle Delta 0.05 %
    Gas Gauging SoH SoH Load Rate 5 hour Rate
    Gas Gauging Turbo Cfg Min Turbo Power 0 cW
    Gas Gauging Turbo Cfg Max C Rate -4 C
    Gas Gauging Turbo Cfg High Frequency Resistance 62 mOhms
    Gas Gauging Turbo Cfg Reserve Energy % 0 %
    Power Power Valid Update Voltage 3500 mV
    Power Shutdown Shutdown Voltage 1750 mV
    Power Shutdown Shutdown Time 10 s
    Power Shutdown PF Shutdown Voltage 1750 mV
    Power Shutdown PF Shutdown Time 10 s
    Power Shutdown Charger Present Threshold 3000 mV
    Power Sleep Sleep Current 10 mA
    Power Sleep Bus Timeout 5 s
    Power Sleep Voltage Time 5 s
    Power Sleep Current Time 20 s
    Power Sleep Wake Comparitor 0 hex
    Power Ship FET Off Time 10 s
    Power Ship Delay 20 s
    Power Ship Auto Ship Time 1440 min
    Power Power Off Debounce 4 250ms
    Power Power Off Timeout 30 min
    Power Manual FET Control MFC Delay 60 s
    PF Status Device Status Data Safety Alert A 0 hex
    PF Status Device Status Data Safety Status A 0 hex
    PF Status Device Status Data Safety Alert B 0 hex
    PF Status Device Status Data Safety Status B 0 hex
    PF Status Device Status Data Safety Alert C 0 hex
    PF Status Device Status Data Safety Status C 0 hex
    PF Status Device Status Data Safety Alert D 0 hex
    PF Status Device Status Data Safety Status D 0 hex
    PF Status Device Status Data PF Alert A 0 hex
    PF Status Device Status Data PF Status A 0 hex
    PF Status Device Status Data PF Alert B 0 hex
    PF Status Device Status Data PF Status B 0 hex
    PF Status Device Status Data PF Alert C 0 hex
    PF Status Device Status Data PF Status C 0 hex
    PF Status Device Status Data PF Alert D 0 hex
    PF Status Device Status Data PF Status D 0 hex
    PF Status Device Status Data Fuse Flag 0 hex
    PF Status Device Status Data Operation Status A 0 hex
    PF Status Device Status Data Operation Status B 0 hex
    PF Status Device Status Data Temp Range 0 hex
    PF Status Device Status Data Charging Status A 0 hex
    PF Status Device Status Data Charging Status B 0 hex
    PF Status Device Status Data Charger Status 0 hex
    PF Status Device Status Data Gauging Status 0 hex
    PF Status Device Status Data IT Status 0 hex
    PF Status Device Voltage Data Cell 1 Voltage 0 mV
    PF Status Device Voltage Data Cell 2 Voltage 0 mV
    PF Status Device Voltage Data Cell 3 Voltage 0 mV
    PF Status Device Voltage Data Cell 4 Voltage 0 mV
    PF Status Device Voltage Data Battery Direct Voltage 0 mV
    PF Status Device Voltage Data Pack Voltage 0 mV
    PF Status Device Current Data Current 0 mA
    PF Status Device Temperature Data Internal Temperature -273.2 degC
    PF Status Device Temperature Data External 1 Temperature -273.2 degC
    PF Status Device Temperature Data External 2 Temperature -273.2 degC
    PF Status Device Temperature Data External 3 Temperature -273.2 degC
    PF Status Device Temperature Data External 4 Temperature -273.2 degC
    PF Status Device Gauging Data Cell 1 Dod0 0 -
    PF Status Device Gauging Data Cell 2 Dod0 0 -
    PF Status Device Gauging Data Cell 3 Dod0 0 -
    PF Status Device Gauging Data Cell 4 Dod0 0 -
    PF Status Device Gauging Data Passed Charge 0 mAh
    PF Status AFE Regs AFE Interrupt Status 0 hex
    PF Status AFE Regs AFE FET Status 0 hex
    PF Status AFE Regs AFE RXIN 0 hex
    PF Status AFE Regs AFE Latch Status 0 hex
    PF Status AFE Regs AFE Interrupt Enable 0 hex
    PF Status AFE Regs AFE FET Control 0 hex
    PF Status AFE Regs AFE RXIEN 0 hex
    PF Status AFE Regs AFE RLOUT 0 hex
    PF Status AFE Regs AFE RHOUT 0 hex
    PF Status AFE Regs AFE RHINT 0 hex
    PF Status AFE Regs AFE Cell Balance 0 hex
    PF Status AFE Regs AFE AD/CC Control 0 hex
    PF Status AFE Regs AFE ADC Mux 0 hex
    PF Status AFE Regs AFE LED Output 0 hex
    PF Status AFE Regs AFE State Control 0 hex
    PF Status AFE Regs AFE LED/Wake Control 0 hex
    PF Status AFE Regs AFE Protection Control 0 hex
    PF Status AFE Regs AFE OCD 0 hex
    PF Status AFE Regs AFE SCC 0 hex
    PF Status AFE Regs AFE SCD1 0 hex
    PF Status AFE Regs AFE SCD2 0 hex
    PF Status AFE Regs AFE Charger Lock 0
    PF Status AFE Regs AFE Charger Voltage 0
    PF Status AFE Regs AFE Charger Current 0
    System Data Manufacturer Data Manufacturer Info A Length 32 -
    System Data Manufacturer Data Manufacturer Info Block A01 61 Hex
    System Data Manufacturer Data Manufacturer Info Block A02 62 Hex
    System Data Manufacturer Data Manufacturer Info Block A03 63 Hex
    System Data Manufacturer Data Manufacturer Info Block A04 64 Hex
    System Data Manufacturer Data Manufacturer Info Block A05 65 Hex
    System Data Manufacturer Data Manufacturer Info Block A06 66 Hex
    System Data Manufacturer Data Manufacturer Info Block A07 67 Hex
    System Data Manufacturer Data Manufacturer Info Block A08 68 Hex
    System Data Manufacturer Data Manufacturer Info Block A09 69 Hex
    System Data Manufacturer Data Manufacturer Info Block A10 6a Hex
    System Data Manufacturer Data Manufacturer Info Block A11 6b Hex
    System Data Manufacturer Data Manufacturer Info Block A12 6c Hex
    System Data Manufacturer Data Manufacturer Info Block A13 6d Hex
    System Data Manufacturer Data Manufacturer Info Block A14 6e Hex
    System Data Manufacturer Data Manufacturer Info Block A15 6f Hex
    System Data Manufacturer Data Manufacturer Info Block A16 70 Hex
    System Data Manufacturer Data Manufacturer Info Block A17 71 Hex
    System Data Manufacturer Data Manufacturer Info Block A18 72 Hex
    System Data Manufacturer Data Manufacturer Info Block A19 73 Hex
    System Data Manufacturer Data Manufacturer Info Block A20 74 Hex
    System Data Manufacturer Data Manufacturer Info Block A21 75 Hex
    System Data Manufacturer Data Manufacturer Info Block A22 76 Hex
    System Data Manufacturer Data Manufacturer Info Block A23 77 Hex
    System Data Manufacturer Data Manufacturer Info Block A24 7a Hex
    System Data Manufacturer Data Manufacturer Info Block A25 78 Hex
    System Data Manufacturer Data Manufacturer Info Block A26 79 Hex
    System Data Manufacturer Data Manufacturer Info Block A27 30 Hex
    System Data Manufacturer Data Manufacturer Info Block A28 31 Hex
    System Data Manufacturer Data Manufacturer Info Block A29 32 Hex
    System Data Manufacturer Data Manufacturer Info Block A30 33 Hex
    System Data Manufacturer Data Manufacturer Info Block A31 34 Hex
    System Data Manufacturer Data Manufacturer Info Block A32 35 Hex
    System Data Integrity Static DF Signature 0 hex
    System Data Integrity Static Chem DF Signature 4671 hex
    System Data Integrity All DF Signature 0 hex
    SBS Configuration Data Remaining AH Cap. Alarm 300 mAh
    SBS Configuration Data Remaining WH Cap. Alarm 432 cWh
    SBS Configuration Data Remaining Time Alarm 10 min
    SBS Configuration Data Initial Battery Mode 81 hex
    SBS Configuration Data Specification Information 31 hex
    SBS Configuration Data Manufacture Date 1/1/1980 date
    SBS Configuration Data Serial Number 1 hex
    SBS Configuration Data Manufacturer Name Texas Instruments -
    SBS Configuration Data Device Name bq40z60 -
    SBS Configuration Data Device Chemistry LION -
    LED Support LED Config LED Delay 100 488us
    LED Support LED Config LED Hold Time 4 s
    LED Support LED Config CHG Thresh 1 25 %
    LED Support LED Config CHG Thresh 2 50 %
    LED Support LED Config CHG Thresh 3 75 %
    LED Support LED Config CHG Thresh 4 100 %
    LED Support LED Config DSG Thresh 1 25 %
    LED Support LED Config DSG Thresh 2 50 %
    LED Support LED Config DSG Thresh 3 75 %
    LED Support LED Config DSG Thresh 4 100 %
    Black Box Safety Status 1st Status Status A 0 hex
    Black Box Safety Status 1st Status Status B 0 hex
    Black Box Safety Status 1st Safety Status C 0 hex
    Black Box Safety Status 1st Safety Status D 0 hex
    Black Box Safety Status 1st Time to Next Event 0 s
    Black Box Safety Status 2nd Status Status A 0 hex
    Black Box Safety Status 2nd Status Status B 0 hex
    Black Box Safety Status 2nd Safety Status C 0 hex
    Black Box Safety Status 2nd Safety Status D 0 hex
    Black Box Safety Status 2nd Time to Next Event 0 s
    Black Box Safety Status 3rd Status Status A 0 hex
    Black Box Safety Status 3rd Status Status B 0 hex
    Black Box Safety Status 3rd Safety Status C 0 hex
    Black Box Safety Status 3rd Safety Status D 0 hex
    Black Box Safety Status 3rd Time to Next Event 0 s
    Black Box PF Status 1st PF Status A 0 hex
    Black Box PF Status 1st PF Status B 0 hex
    Black Box PF Status 1st PF Status C 0 hex
    Black Box PF Status 1st PF Status D 0 hex
    Black Box PF Status 1st Time to Next Event 0 s
    Black Box PF Status 2nd PF Status A 0 hex
    Black Box PF Status 2nd PF Status B 0 hex
    Black Box PF Status 2nd PF Status C 0 hex
    Black Box PF Status 2nd PF Status D 0 hex
    Black Box PF Status 2nd Time to Next Event 0 s
    Black Box PF Status 3rd PF Status A 0 hex
    Black Box PF Status 3rd PF Status B 0 hex
    Black Box PF Status 3rd PF Status C 0 hex
    Black Box PF Status 3rd PF Status D 0 hex
    Black Box PF Status 3rd Time to Next Event 0 s
    Lifetimes Voltage Cell 1 Max Voltage 0 mV
    Lifetimes Voltage Cell 2 Max Voltage 0 mV
    Lifetimes Voltage Cell 3 Max Voltage 0 mV
    Lifetimes Voltage Cell 4 Max Voltage 0 mV
    Lifetimes Voltage Cell 1 Min Voltage 32767 mV
    Lifetimes Voltage Cell 2 Min Voltage 32767 mV
    Lifetimes Voltage Cell 3 Min Voltage 32767 mV
    Lifetimes Voltage Cell 4 Min Voltage 32767 mV
    Lifetimes Voltage Max Delta Cell Voltage 0 mV
    Lifetimes Current Max Charge Current 0 mA
    Lifetimes Current Max Discharge Current 0 mA
    Lifetimes Current Max Avg Dsg Current 0 mA
    Lifetimes Current Max Avg Dsg Power 0 cW
    Lifetimes Temperature Max Temp Cell -128 degC
    Lifetimes Temperature Min Temp Cell 127 degC
    Lifetimes Temperature Max Delta Cell Temp 0 degC
    Lifetimes Temperature Max Temp Int Sensor -128 degC
    Lifetimes Temperature Min Temp Int Sensor 127 degC
    Lifetimes Temperature Max Temp Fet -128 degC
    Lifetimes Safety Events No Of COV Events 0 events
    Lifetimes Safety Events Last COV Event 0 cycles
    Lifetimes Safety Events No Of CUV Events 0 events
    Lifetimes Safety Events Last CUV Event 0 cycles
    Lifetimes Safety Events No Of OCD1 Events 0 events
    Lifetimes Safety Events Last OCD1 Event 0 cycles
    Lifetimes Safety Events No Of OCD2 Events 0 events
    Lifetimes Safety Events Last OCD2 Event 0 cycles
    Lifetimes Safety Events No Of OCC1 Events 0 events
    Lifetimes Safety Events Last OCC1 Event 0 cycles
    Lifetimes Safety Events No Of OCC2 Events 0 events
    Lifetimes Safety Events Last OCC2 Event 0 cycles
    Lifetimes Safety Events No Of AOLD Events 0 events
    Lifetimes Safety Events Last AOLD Event 0 cycles
    Lifetimes Safety Events No Of ASCD Events 0 events
    Lifetimes Safety Events Last ASCD Event 0 cycles
    Lifetimes Safety Events No Of ASCC Events 0 events
    Lifetimes Safety Events Last ASCC Event 0 cycles
    Lifetimes Safety Events No Of OTC Events 0 events
    Lifetimes Safety Events Last OTC Event 0 cycles
    Lifetimes Safety Events No Of OTD Events 0 events
    Lifetimes Safety Events Last OTD Event 0 cycles
    Lifetimes Safety Events No Of OTF Events 0 events
    Lifetimes Safety Events Last OTF Event 0 cycles
    Lifetimes Charging Events No Valid Charge Term 0 events
    Lifetimes Charging Events Last Valid Charge Term 0 cycles
    Lifetimes Gauging Events No Of Qmax Updates 0 events
    Lifetimes Gauging Events Last Qmax Update 0 cycles
    Lifetimes Gauging Events No Of Ra Updates 0 events
    Lifetimes Gauging Events Last Ra Update 0 cycles
    Lifetimes Gauging Events No Of Ra Disable 0 events
    Lifetimes Gauging Events Last Ra Disable 0 cycles
    Lifetimes Power Events No Of Shutdowns 0 events
    Lifetimes Cell Balancing Cb Time Cell 1 0 h
    Lifetimes Cell Balancing Cb Time Cell 2 0 h
    Lifetimes Cell Balancing Cb Time Cell 3 0 h
    Lifetimes Cell Balancing Cb Time Cell 4 0 h
    Lifetimes Time Total Fw Runtime 0 h
    Lifetimes Time Time Spent In UT 0 h
    Lifetimes Time Time Spent In LT 0 h
    Lifetimes Time Time Spent In STL 0 h
    Lifetimes Time Time Spent In RT 0 h
    Lifetimes Time Time Spent In STH 0 h
    Lifetimes Time Time Spent In HT 0 h
    Lifetimes Time Time Spent In OT 0 h
    Ra Table R_a0 Cell0 R_a flag 0 -
    Ra Table R_a0 Cell0 R_a 0 85 2^-10ohm
    Ra Table R_a0 Cell0 R_a 1 35 2^-10ohm
    Ra Table R_a0 Cell0 R_a 2 42 2^-10ohm
    Ra Table R_a0 Cell0 R_a 3 50 2^-10ohm
    Ra Table R_a0 Cell0 R_a 4 48 2^-10ohm
    Ra Table R_a0 Cell0 R_a 5 37 2^-10ohm
    Ra Table R_a0 Cell0 R_a 6 48 2^-10ohm
    Ra Table R_a0 Cell0 R_a 7 52 2^-10ohm
    Ra Table R_a0 Cell0 R_a 8 51 2^-10ohm
    Ra Table R_a0 Cell0 R_a 9 54 2^-10ohm
    Ra Table R_a0 Cell0 R_a 10 59 2^-10ohm
    Ra Table R_a0 Cell0 R_a 11 94 2^-10ohm
    Ra Table R_a0 Cell0 R_a 12 197 2^-10ohm
    Ra Table R_a0 Cell0 R_a 13 306 2^-10ohm
    Ra Table R_a0 Cell0 R_a 14 411 2^-10ohm
    Ra Table R_a1 Cell1 R_a flag 0 -
    Ra Table R_a1 Cell1 R_a 0 89 2^-10ohm
    Ra Table R_a1 Cell1 R_a 1 37 2^-10ohm
    Ra Table R_a1 Cell1 R_a 2 40 2^-10ohm
    Ra Table R_a1 Cell1 R_a 3 47 2^-10ohm
    Ra Table R_a1 Cell1 R_a 4 46 2^-10ohm
    Ra Table R_a1 Cell1 R_a 5 36 2^-10ohm
    Ra Table R_a1 Cell1 R_a 6 47 2^-10ohm
    Ra Table R_a1 Cell1 R_a 7 51 2^-10ohm
    Ra Table R_a1 Cell1 R_a 8 52 2^-10ohm
    Ra Table R_a1 Cell1 R_a 9 56 2^-10ohm
    Ra Table R_a1 Cell1 R_a 10 62 2^-10ohm
    Ra Table R_a1 Cell1 R_a 11 104 2^-10ohm
    Ra Table R_a1 Cell1 R_a 12 211 2^-10ohm
    Ra Table R_a1 Cell1 R_a 13 324 2^-10ohm
    Ra Table R_a1 Cell1 R_a 14 437 2^-10ohm
    Ra Table R_a2 Cell2 R_a flag 0 -
    Ra Table R_a2 Cell2 R_a 0 82 2^-10ohm
    Ra Table R_a2 Cell2 R_a 1 34 2^-10ohm
    Ra Table R_a2 Cell2 R_a 2 41 2^-10ohm
    Ra Table R_a2 Cell2 R_a 3 49 2^-10ohm
    Ra Table R_a2 Cell2 R_a 4 48 2^-10ohm
    Ra Table R_a2 Cell2 R_a 5 38 2^-10ohm
    Ra Table R_a2 Cell2 R_a 6 49 2^-10ohm
    Ra Table R_a2 Cell2 R_a 7 54 2^-10ohm
    Ra Table R_a2 Cell2 R_a 8 54 2^-10ohm
    Ra Table R_a2 Cell2 R_a 9 57 2^-10ohm
    Ra Table R_a2 Cell2 R_a 10 62 2^-10ohm
    Ra Table R_a2 Cell2 R_a 11 98 2^-10ohm
    Ra Table R_a2 Cell2 R_a 12 209 2^-10ohm
    Ra Table R_a2 Cell2 R_a 13 532 2^-10ohm
    Ra Table R_a2 Cell2 R_a 14 718 2^-10ohm
    Ra Table R_a3 Cell3 R_a flag 0 -
    Ra Table R_a3 Cell3 R_a 0 82 2^-10ohm
    Ra Table R_a3 Cell3 R_a 1 34 2^-10ohm
    Ra Table R_a3 Cell3 R_a 2 41 2^-10ohm
    Ra Table R_a3 Cell3 R_a 3 48 2^-10ohm
    Ra Table R_a3 Cell3 R_a 4 47 2^-10ohm
    Ra Table R_a3 Cell3 R_a 5 37 2^-10ohm
    Ra Table R_a3 Cell3 R_a 6 47 2^-10ohm
    Ra Table R_a3 Cell3 R_a 7 52 2^-10ohm
    Ra Table R_a3 Cell3 R_a 8 54 2^-10ohm
    Ra Table R_a3 Cell3 R_a 9 57 2^-10ohm
    Ra Table R_a3 Cell3 R_a 10 63 2^-10ohm
    Ra Table R_a3 Cell3 R_a 11 101 2^-10ohm
    Ra Table R_a3 Cell3 R_a 12 217 2^-10ohm
    Ra Table R_a3 Cell3 R_a 13 332 2^-10ohm
    Ra Table R_a3 Cell3 R_a 14 450 2^-10ohm
    Ra Table R_a0x xCell0 R_a flag 55 -
    Ra Table R_a0x xCell0 R_a 0 85 2^-10ohm
    Ra Table R_a0x xCell0 R_a 1 35 2^-10ohm
    Ra Table R_a0x xCell0 R_a 2 42 2^-10ohm
    Ra Table R_a0x xCell0 R_a 3 50 2^-10ohm
    Ra Table R_a0x xCell0 R_a 4 48 2^-10ohm
    Ra Table R_a0x xCell0 R_a 5 37 2^-10ohm
    Ra Table R_a0x xCell0 R_a 6 48 2^-10ohm
    Ra Table R_a0x xCell0 R_a 7 52 2^-10ohm
    Ra Table R_a0x xCell0 R_a 8 51 2^-10ohm
    Ra Table R_a0x xCell0 R_a 9 54 2^-10ohm
    Ra Table R_a0x xCell0 R_a 10 59 2^-10ohm
    Ra Table R_a0x xCell0 R_a 11 94 2^-10ohm
    Ra Table R_a0x xCell0 R_a 12 197 2^-10ohm
    Ra Table R_a0x xCell0 R_a 13 313 2^-10ohm
    Ra Table R_a0x xCell0 R_a 14 420 2^-10ohm
    Ra Table R_a1x xCell1 R_a flag 55 -
    Ra Table R_a1x xCell1 R_a 0 89 2^-10ohm
    Ra Table R_a1x xCell1 R_a 1 37 2^-10ohm
    Ra Table R_a1x xCell1 R_a 2 40 2^-10ohm
    Ra Table R_a1x xCell1 R_a 3 47 2^-10ohm
    Ra Table R_a1x xCell1 R_a 4 46 2^-10ohm
    Ra Table R_a1x xCell1 R_a 5 36 2^-10ohm
    Ra Table R_a1x xCell1 R_a 6 47 2^-10ohm
    Ra Table R_a1x xCell1 R_a 7 51 2^-10ohm
    Ra Table R_a1x xCell1 R_a 8 52 2^-10ohm
    Ra Table R_a1x xCell1 R_a 9 56 2^-10ohm
    Ra Table R_a1x xCell1 R_a 10 62 2^-10ohm
    Ra Table R_a1x xCell1 R_a 11 104 2^-10ohm
    Ra Table R_a1x xCell1 R_a 12 211 2^-10ohm
    Ra Table R_a1x xCell1 R_a 13 331 2^-10ohm
    Ra Table R_a1x xCell1 R_a 14 446 2^-10ohm
    Ra Table R_a2x xCell2 R_a flag 55 -
    Ra Table R_a2x xCell2 R_a 0 82 2^-10ohm
    Ra Table R_a2x xCell2 R_a 1 34 2^-10ohm
    Ra Table R_a2x xCell2 R_a 2 41 2^-10ohm
    Ra Table R_a2x xCell2 R_a 3 49 2^-10ohm
    Ra Table R_a2x xCell2 R_a 4 48 2^-10ohm
    Ra Table R_a2x xCell2 R_a 5 38 2^-10ohm
    Ra Table R_a2x xCell2 R_a 6 49 2^-10ohm
    Ra Table R_a2x xCell2 R_a 7 54 2^-10ohm
    Ra Table R_a2x xCell2 R_a 8 54 2^-10ohm
    Ra Table R_a2x xCell2 R_a 9 57 2^-10ohm
    Ra Table R_a2x xCell2 R_a 10 62 2^-10ohm
    Ra Table R_a2x xCell2 R_a 11 98 2^-10ohm
    Ra Table R_a2x xCell2 R_a 12 209 2^-10ohm
    Ra Table R_a2x xCell2 R_a 13 525 2^-10ohm
    Ra Table R_a2x xCell2 R_a 14 709 2^-10ohm
    Ra Table R_a3x xCell3 R_a flag 55 -
    Ra Table R_a3x xCell3 R_a 0 82 2^-10ohm
    Ra Table R_a3x xCell3 R_a 1 34 2^-10ohm
    Ra Table R_a3x xCell3 R_a 2 41 2^-10ohm
    Ra Table R_a3x xCell3 R_a 3 48 2^-10ohm
    Ra Table R_a3x xCell3 R_a 4 47 2^-10ohm
    Ra Table R_a3x xCell3 R_a 5 37 2^-10ohm
    Ra Table R_a3x xCell3 R_a 6 47 2^-10ohm
    Ra Table R_a3x xCell3 R_a 7 52 2^-10ohm
    Ra Table R_a3x xCell3 R_a 8 54 2^-10ohm
    Ra Table R_a3x xCell3 R_a 9 57 2^-10ohm
    Ra Table R_a3x xCell3 R_a 10 63 2^-10ohm
    Ra Table R_a3x xCell3 R_a 11 101 2^-10ohm
    Ra Table R_a3x xCell3 R_a 12 217 2^-10ohm
    Ra Table R_a3x xCell3 R_a 13 339 2^-10ohm
    Ra Table R_a3x xCell3 R_a 14 459 2^-10ohm
  • Cliff
    I need the actual gg.csv file. If the e2e expands it, then maybe you can zip it before uploading.

    Tom
  • Tom

    I am trying to figure out how to upload to this forum without expanding it.

    Cliff