Hi Team,
Would it be safe to generate ~1.2A at +1.0Vdc from a worst case input voltage of +20Vdc with this part? If there are any risks, please let me know -- thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Would it be safe to generate ~1.2A at +1.0Vdc from a worst case input voltage of +20Vdc with this part? If there are any risks, please let me know -- thanks!
1 V from 20 V requires about 5% duty cycle. 110 nsec ton min typ and 400 kHz Fsw typ give 4.4 % min duty cycle. Fsw max gives 5.61% minimum duty cycle. Assuming that the maximum typical on time is about 135 nsec (may be more, it is not specified), you could have minimum duty cycle of 6.89 %. Do you care if you skip pulses?
I don't see anything. Even webench does not show any loop response data. Somewhat surprising as the is a current mode control device. Just FYI though, I do not support TPS54302 directly. As you may know, I answer a lot of general questions on e2e. If I know the answer it is faster just to answer the post than trying to track down someone else to answer.