This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27761: LM27761 specification about Vin and Vout

Part Number: LM27761


Hello team,

I designed as the following voltage using LM27761
Vin = 5.0V, Vout = -5.0V
So I found the following noise which is more than switching noize.  This noize level is  almost 70mV.
If I set the Vin voltage is 5.1V, so this noise disappears. So I am thinking that Vin voltage should be increased than 5.1V.

My question is the following. 
How much  shoud I increase at least about Vin Voltage?

Best Regards,
Akihisa Tamazaki