I would like to confirm the cause of the unexpected output in EN low for TPS799-Q1.
I attached the waveform.
The conditon is VIN = 3.3V, EN = 2.7V, input capacitor 4.7uF and output capacitor 2.2uF.
The output voltage in EN low was about 0.5V.
When input voltage was 2.7V, there was not output voltage.
What is the cause of it ?
Is it correct operation?
Best regards,
Atsushi Yamauchi