Other Parts Discussed in Thread: TLV61046
There have been 2 threads that have mentioned the TLV61046, which seems to be a larger packaged (SOT) TPS61046. I have been trying to get information (via other avenues than posting on E2E) on samples, availability, datasheet, etc, and have come up empty, so I'm giving E2E a shot.
I've designed around the TPS61046, as it has the necessary features and cost, but from an inexpensive PCB manufacturing point of view, it doesn't quite fit the bill as well as an SOT would. Also, selecting an inductor that can handle the limits of current of the TPS61046 results in quite a large inductor, so I'm not fully comprehending the advantage of such a small package that the TPS61046 is available in.
Any help would be greatly appreciated.