This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24172 charge setting

Part Number: BQ24172

Dear Sir,

So far, we are using CHARGER BQ24172 for our system.

so far, we are measuring our battery capacity. we have got some problem below

1. Our battery can not be charge to 100% . our Icharge=1.7A  , so the Iterm shoule be 170mA (1/10 Icharge).  so far we found Icharge = 260mA then it will jump to 0mA and will not keep charging (as below battery charge time table). Can I revise the Ich cut off point?

2. Cell voltage adjustment: Our Actual cell voltage is 4.241V. we want to adjust to near 4.2V. may I know how to adjust it ?

Thanks.