Part Number: BQ27441-G1
Hello All,
I am implementing the recommended flowchart which is figure 3 of the QuickStart Guide. After some analysis, I have the following questions:
- The idea is that when QMAX and resistance profiles are updated, the host processor should store the values in non volatile memory. Then, when the configuration parameters are sent to the Gauge (fig 1), these two should be updated as well. Is this correct?
- Does it make sense that the system go from "Figure 1" to check QMAX flag? Should not it go directly to normal operation and then check if the values should be stored when the system entered/exited discharge and ITPOR != 1?
Thanks.