Hello,
I am using bq76pl455AQ1 for EV application.The IC works fine when the battery is not connected to a charger.But due to some reason, it burns when I connect a constant current charger to the battery pack.
Specs: 52 Li-ion cells 13 series and 4 parallel
Constant charging current: 3A
Connections are exactly according to the datasheet specs.LPF contains 1k resistor and 1uF capacitor.
Any help would be highly appreciated
Thank you!