This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2491: Can I reduce C1 value? What is the min?

Part Number: TPS2491

Hi Team,

In both datasheet and design tool, I notice C1 is fixed at 0.1uF. Can I reduce this capacitance value? What is the minimum value? Current input is 48V and 4.4A inrush current is observed. With that, connector pins tend to be spoilt after hundred plugging action. If C1 is replaced with 0.01uF, 2A inrush current is observed. Kindly advise.

Thanks.

- YY