Hi:
I have look for the VFC in the datasheet of bq2060a, Howerver , there is no mention of the details.
1. How about the VFC get Vdd from? Can anyone give me the block to decript it?? If the external JFET generate a wave drift about 30mV.(Vcc is in the range of 3.1-3.5), does it will affect the VFC frequency?
2. Does the external capacity in bq2060a will affect the VFC work. for capacity venting?
2.1) One sample, I calibrate the VFC in the alternate mode, VFC value increase while i continues re-calibrate the battery... I am very sure i have correctly calibrate the voltage. If apply a discharge current to the battery. several minutes later, re-calibrate the battery VFC in the alternate mode, The VFC value is very small with 100(100 in dec). What could i to do futher???