I have questions about TPS65251.
Question 1.
Please tell me the output voltage temperature characteristic of the TPS65251.
Example) _% Vout/℃
Question 2.
In datasheet P.6(Load regulation - DC ΔVOUT/ΔIOUT),
Does it mean that output voltage shifts by 0.5% when output current is 3A?
Question 3.
In datasheet P.6(Line regulation - DC ΔVOUT/ΔVINB),
Does it mean that 0.5% of output voltage shifts when voltage changes from 4.5V to 18V?