This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/BQ40Z60: Linux Driver

Part Number: BQ40Z60

Tool/software: Linux

Hi,

I would like to know if there is a Linux driver for the BQ40Z60 available that supports SMBus Block Write and Block Read functionality.

The current driver I am using supports only the following features:

SMBus Quick Command              no
SMBus Send Byte                  yes
SMBus Receive Byte               yes
SMBus Write Byte                 yes
SMBus Read Byte                  yes
SMBus Write Word                 yes
SMBus Read Word                  yes
SMBus Process Call               no
SMBus Block Write                no
SMBus Block Read                 no
SMBus Block Process Call         no

It would save me some time to get a verified driver which supports all SMB features rather than modifying the existing driver.


Thanks for the help!


Fred