Other Parts Discussed in Thread: BQSTUDIO
I'm using BQ40Z60EVM-578 to evaluate our NCR 18650B, lithium Ion battery, 4 series, so the final output is 3.7v*4.
Power supply: BK precision 1762 DC power supply. Set output to 20V, current output is set to max.
Load: 40ohm resistor.
I just found an issue regarding not resuming charge. The battery pack was fully charged, and partially discharged around 2481mAh(remaining capacity). Then I turned on the external power supply, but it seems it won't resume charging as the charging current is 0mA. The external power supply only supply power to the resistor load.
I attached my log and data memory export.unable to charge after partial discharge.zip
Any idea?