Hi everybody,
we have built an LED driver based on the TPS61199 powered by 12V (VIN). The control of EN and PWM is done by a microcontroller powered by 5V. Everything works fine.
Now the problem: We want to change the input voltage to 24V, so the input capacitors, inductance and current sense resistors were changed to support the new input voltage. The control of EN and PWM is still done by the microcontroller powered by 5V. The problem is as soon as the microcontroller pulls the EN pin to 5V the driver burns and is dead.
I did some testing with the TPS61199 Eval Board (EVM-598): On this board the TPS61199 works with 24V Vin -> on the board there is a resistor divider to scale the input voltage to 2/3 for the EN Pin so with 24V VIN the EN voltage is at 16V.
After finding this out I disconnected the microcontroller on our LED driver from the EN pin and inserted the resistor divider as it is on the eval board -> result is the driver does not burn and works.
Why does the TPS61199 die immediately when I apply the 5V on the EN Pin? This pin should be a logic input and not be related to VIN.
Any suggestions?
Best regards,
Stefan