This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5088: webench 48V to 12V 8A switcher, excessive heat?

Part Number: LM5088
Other Parts Discussed in Thread: LM5117

Hi, I'm new to switcher circuits and I'm prototyping a 48V to 12V 8A buck provided by webench, link below.

https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=A5CA048BF3A3E950

The fet and inductor are getting rather hot at relatively low currents and was wondering if I could bounce this on here for any suggestions.
Ambient temperature is 24 oC, purely resistive loads and PCB without any heatsinks sitting flat on table for all tests.

----

With a 22R load
48V @ 0.16A
12V @ 0.545A
After 15mins the inductor and fet go to around 49 oC

---

With a 10R load

48V @ 0.35A

12V @ 1.2A

After 15mins the inductor and fet go to around 69 oC

---

With a 3R3 load

48V @ 1.15A

12V @ 3.64A

After 5mins the fet goes to 132oC and rising

---

I was thinking this seems a little excessive without heatsinking?
After I figure it out, I'll upload the PCB layout and scope traces on here which would be useful.

The Gate waveform seems to not be a clean pwm signal, rather it also has some odd signals on there and was leading me to wonder if the fet was being driven in its linear region.
On first glance these don't seem to being fed through to the inductor.

Thanks for any thoughts on this,

Jerome