Other Parts Discussed in Thread: EV2400
I am considering using the bq28z610 device for a 2s pack.
I already have the Gauge Development Kit which I was hoping to use to create a golden image but as I am using 2 cells in series, I think I will not be able to charge and discharge the two cells as the kit does not support the voltage levels.
Is there a way to perform a golden image on one cell and translate that to two cells in series? Otherwise what is the best way to automate creating a golden image?
Thanks
Trev