Hi,
Hope to know the behavior of the current limit function, here below is the scenario :
1) DC/DC output voltage set to 10V
2) Load is a resistive load, like a 10 ohm resistor
3) Current limit is set to 0.5A
In this case, will the DC/DC circuit output 5V @0.5A ?
And if the resistive load is like a 100 ohm resistor, the circuit will output 10V, and consuming 0.1A in the load side ?
Thanks.