I want to create a sync signal for a TPS54618. I'm going to drive a 400 kHz square wave sync signal but it's going to take a while for the 400 kHz signal to turn on, so until it's up and running I have a 511K resistor from the RT/CLK pin to this held-low sync signal that will later be generating a square wave. Will the power supply come up and operate at 400 kHz if the 511K resistor is going to a held-low CMOS 3.3V output signal? And once my sync signal starts oscillating, will there be a blip on the output power rail as the sync signal starts up?