This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: Accuracy of Alert pin frequency

Part Number: BQ76930

In "ALWAYS ON" mode, what is the accuracy of the 250 msec Alert pin?

We found that it's accuracy was off by about 2%.

This was tested by counting the Alert pin pulses over a one hour interval and comparing it to an Atomic clock.

BQ76930 DOC REF:

7.3.1.1.3 16-Bit CC
In ALWAYS ON mode, the CC runs at 100%, gathering a fresh reading every 250 ms. The conclusion of each reading sets the CC_READY bit, which toggles the ALERT pin high to inform the microcontroller that a new reading is available. To enable Always On mode, set [CC_EN] = 1.