This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC33063A: Light load support

Part Number: MC33063A
Other Parts Discussed in Thread: TPS54140A

Hi,

One of my customers is using the IC for a buck application.

Vin-11V to 33V DC, 

Vout- 3.3V at 1A peak current. The normal load will be around 0.3A to 0.5A

During sleep mode, the IC needs to source around 20mA.

Does this device work at a good efficiency at these light loads? if not can you suggest an alternative at the similar cost?

I was thinking that TPS54140A would be a better fit.