Other Parts Discussed in Thread: TPS61178, TPS62180, DRV8305, CSD25304W1015
Hello,
I am currently working on the power supply for our on-going project, where there are some brushless DC motors in use.
This device we get here is a pretty good solution we believe, however this shutdown mode could not completely turn off the output. We evaluate the solution with the evaluation board, giving the input voltage 3.7V, and the output voltage is tuned to 9V. Fair enough! But we saw that when we set EN pin low, the output was dropped to around 3.3V instead of 0V as we expected. I learned that for some of the other devices, of which there is load disconnection, they could probably shut the output power off. Am I right? But then what is the purpose of having this EN pin, just to save the power?
How could we do if we would like to completely disconnect the output power in the shutdown mode then?
Thanks in advance!