Hi
I have a question about the pull-up voltage of FLAGx pin.
At the datasheet, the recommend voltage of FLAGx pin is -0.3V~VCC+0.3V. However the abs max is -0.3V~6.0V.
Is it possible the FLAGx pin is pulled up to 5V when the VCC is applied by another supply (e.g 3.3V)?
I refereed the following post.
https://e2e.ti.com/support/power_management/svs_and_sequencers/f/212/t/551649
In this case, the voltage of FLAG pin does not exceed the abs max. However it is exceeded the recommend voltage.
Regards,
Koji Hamamoto