This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25910: lower operational current

Part Number:


We are thinking of using the TPS25910 as a "high-side protection switch" for our system (Vin = 15V max, Iout = 5A max).  I have used the dev board (TPS25910EVM) and it tests out fine for all of our typical use cases, EXCEPT one. . . . .  operation current which is 5mA maximum (2.5mA typ in "OFF").  This is too high for our system.  I can work around this by switching Vin ON/OFF before getting to the TPS25910; however, would love to be able to not do this.  So. . .  is there another part of comparable price, form factor, and operation that has a much lower operation current (~10uA or less).

Thanks,

Dave Brobst