Other Parts Discussed in Thread: LM2677, LM25085A
Hello,
I have design a power supply 29V AC input to 24V 5A output.
I have use the TI webench for choice my component.
In the TI webench, it say 2.8mV of noise.
I have design my board in suiting the TI recommendation, i have see the TI documentation about noise "www.ti.com/lit/an/slyt682/slyt682.pdf"
I have test my board, (0.7A and 1.5A) i have 190mV of noise HF, the frequency is 50Mhz. The noise appear when the SW pin change.
The switching frequency is 129Khz, the output capacitor is low ESR
My schematic:
My PCB: the board have 2 layer and copper thickness is 70µm.
The oscillo picture:
HF noise
Decoupling frequency:
I have test to change self, to shielded self, no amelioration.
I have change the STPS20M100S diode to other diode (TPS5100-13) but the noise is increase.
Do you have solution for reduce HF noise?
Thanks