Other Parts Discussed in Thread: TINA-TI, , , UCC3895
Tool/software: TINA-TI or Spice Models
How design the external circuit of peak current control mode with UCC2895 in shifting phase full bridge?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Oliver!
I'm really appreciate for your help! I study the datasheet and user's guide again,and get some questions.
1. The output of the small transistor connect a resistor to the RAMP, how to design the value of this resistor?
2. Assume the VBE=0.7V, it means that only the voltage of sawtooth above the 0.7V, the RAMP footprint can get the voltage. This will result in the duty ratio jump in smaller duty cycle, is there any methods to solve this problems?
3.The ADS and CS footprint has a resistor respectively, how to confirm the value level?
4.This is my control schematic, please help me check it out.
Thank you!
Hi Qi,
The calculation of slope compensation components is suggested on page 3-106 and 3-107 of U-111, the app-note describes the whole details better than I can. For the ADS configuration, please use equation 5&6 in the datasheet to determine the resistors divider. The resistor value should as large as possible to avoid sourcing too much current from CS but need to provide enough bias current(+-20µA) for this pin.
Thanks
Oliver