This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL2844B: Regarding maximum power dissipation of PWM controller

Part Number: TL2844B


Hi,

We are planning to replace UC2844ADM (from Microsemi) with TL2844BD-8 (got this from TI crossreference search) in one of our projects.

I would like to know the maximum power dissipation at ambient temperature of 25 deg C for TL2844BD-8.

The datasheet provides a formula to calculate based on thermal resistance, TJ and TA, but does not provide any information related to max power dissipation either in operating or absolute maximum ratings.

Can you please let me know TL2844BD-8 maximum power dissipation?  Is it 1W max?

Also, can you please let me know the part life cycle status in terms of number of years for TL2844BD-8?  I know that this product is active, but wanted to know the duration.

Awaiting for your reply.

Regards,

Archana Rao

  • Hello Archana,

    This has to do with the ambient temperature of the design and the maximum junction temperature device and the device’s thermal impedance theta JA (Rja) and the ambient temperature you are using.

    The 8 pin D package has an Rja of 97 deg. C/W and a maximum junction temperature of 150 C. At 80 degree C ambient the maximum power would be 720 mW.

    Tjmax = Tamb +Pmax*Rja

    Pmax = (Tjmax-Tamb)/Rja = (150-80)/97 = 720 mW

    Regards,

    Mike

  • Hi Mike,

    Thank you for your reply.

    The information provided was very helpful.  Can I consider that at -40deg C, the device can handle up to 1.96W of power dissipation assuming that max junction temperature  is 150 degC?

    Regards,

    Archana Rao

  • Hello Archana,

    Your calculation is correct.  I might reduce the 150 degree C to 125 degree C in your calculation for design margin.

    This would put the absolute maximum at -40 C at 1.7W.

    Regards,

    Mike