Other Parts Discussed in Thread: TIDA-00653
Tool/software: Code Composer Studio
Hi All,
We want to kick off a project for E-bike DC/DC converter,the TIDA-00653 is available,the configuration of our production
as below:input voltage:6-13.6V,output voltage:36V,the power is 500W;
now we have some issue :
1、If the input voltage(6-13.6V) is available in the TIDA-00653 EVM?how many the range of the input voltage?
2、If there are some training for the circuit diagram and PCB Layout?
3、Can you help to show us the link of software for the EVM?
Very thanks for your help.