Hello all, I have a project with positive and negative supply rails. The TL720M05-Q1 regulates the positive input supply from +7V to +5V, and a negative regulator regulates another input supply from -12V to -10V. There are some biasing resistors connecting the +5V rail to the -10V rail. I've noticed that if I apply the -12V input whithout the +7V input, the -10V rail starts fine, and pulls the +5V down to around -0.47V through some of those biasing resistors. If I then apply the +7V input, the TL720M05-Q1 will not start, and its +5V output rail will remain at -0.47.
If I apply the +7V input before the -12V input, then both LDOs start fine, but I need to be able to deal with both possibilities. I presume it's something with the TL720M05-Q1's internal reverse polarity protection, but the datasheet does not any details.
Please advise.
Mike Twieg