Hello,
I am working with the LM3150 using the BSC059N04LS as my low side MOSFET. I have not been able to get the current limit to trip even when both my calculations and scope captures suggest that it should be tripping and as a result skipping cycles to try and recover.
Input Current |
.2A |
Input Wattage (I * 27V) |
5.4W |
@85% efficiency, Output Wattage |
4.6W |
Output current (output W/4.3V) |
1A |
Resistor (ILIM) |
43 Ohm |
Here is a capture of the ILIM pin voltage (CH2) and the voltage across the low side FET (CH1). The FET voltage is clearly higher than the ILIM set voltage but the next cycle is not skipped.
I am running out of ideas for why this part is not operating the way it seems like it should.
Note: There is a Feed-forward capacitor, Ripple Injection Network across the inductor to FB, and a snubber in this set up. Have any of these additional circuits shown to interfere with the current limit functionality?