This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Requirement of Power Management IC

Hello,

I require a Power Management IC which can switch between my two inputs (main power input  5V and Primary backup battery 3.6V).

When the main power supply is present then the output of the Power Management IC should be from main power and when main power supply is absent then the battery backup should operate.

Please suggest  suitable part which suffice the requirement.

Thanks and Regards,
NIBIN DAS S
iWave Systems Technologies Pvt Ltd
No. 7/B, 29th Main, BTM Layout 2nd Stage,
Bangalore - 560 076.
Mob No:+91-8129639910
Skype ID : Nibindass
Phone: +91-80-26786245, 26683700