This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV702: /EN pin current

Part Number: TLV702

Hi, with TLV70233DBVR

I am using a 10k resistor to pull /EN to Vin
however the Vout is only 1.3V
when I use a 1k resistor to pull up /EN the voltage goes up to 2.9V
finally when I short /EN to Vin I get the full desired 3.3V output
The specsheet says that EN pin only needs less than 1uA so I am confused, please help.