This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Survey DC/DC LED Driver

Other Parts Discussed in Thread: TPS92691, TPS92691EVM-752

Hi Sir,

We have LED Driver request.

Could you help provide solution can meet as below spec ? Thanks,

1.    Input voltage 25.4Vdc, output voltage 27-48Vdc can be adjustable (control signal is from 0 to 3.0V respectively). If IC can’t adjust its output voltage directly, we may add additional circuit by ourselves.

2.    Output current: 0-4.7A.

3.    Suggestion Vcc=12V.

4.    Current mode control, main MOSFET current can be limited cycle by cycle.

5.    Expecting Operating frequency: 100kHz-200kHz.

6.    Soft start function.

7.    Better to have output OVP and input UVP detection function. Output OVP need to latch while input UVP is auto-recovery type.

8.    Good dynamic response to pulse load (refer to LED current at 3D TV mode).

9.    Package: SMD type, SOIC or others.