Other Parts Discussed in Thread: BQ25892
Hello,
I am working implementing the BQ24250 but I have a few questions that I have not been able to find in past posts or through the datasheet.
1) Would there be a concern regarding cell capacity with this charger (besides temperature as noted in the datasheet)? The project will be a re-use type idea that will have a single cell with an anticipated capacity of 10Ah. From conversations, it sounds like that they cells are a 1S3P configuration, and may be challenging to separate a single cell out. This would mean a potential 30Ah capacity, are there concerns with using this for such a large capacity? The project is meant to be low current applications (2Amps in or out).
I have read about the self-timeout of 6hours default, so I do understand that this would need to be disabled to achieve the required duration to fully charge.
2) The cells are second use so their Regulated Voltage is target at 4.1V. This would require adjusting Register #3 VBATREG. The problem is I cannot understand how I would appropriately configure that register to achieve a 4.1V regulated voltage. I would assume that setting any of the VBATREG registers TRUE would indicate an offset to the 4.44 maximum VBATREG. Based on what is defaulted in the registers (640mV/40mV/20mV = 720mV offset), and the default Regulated Voltage of 4.2V, I do not understand how to set this register to achieve 4.1V. What would be the proper way to configure?
3) Since I will be using the I2C for configuration (I do not plan to use the Watchdog), are the registers retained across Loss of Power to the BQ24250 (Volatile vs. non-volatile)? Or would they need to be configured if power is lost?
Thank you for the support on these questions!
Wayne