This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR64010: When fz of LMR64010 became close the recommended range, behavior disstability. Is there a problem?

Part Number: LMR64010

Dear supportmember,

My customer use LMR64010.

I have two question.


Q1
Although fz is recommend 8kHz description of datasheet,
when fz became close 8kHz, Ripple voltage became 4V and behavior disstability.

Is it correct as a phenomenon?


Q2
When fz is 0.6~2.1kHz decrease,
Ripple voltage became 27mV and behavior stability.

Is fz correct as setting 0.6~2.1kHz,
Is fz problem as setting?


(Specification condition)
Vin: 5V
Vout :28V
Iout: 0.01A

R1 :283kΩ
R2 :13kΩ
Cff: 82pF

Fz:6.9kHz

L :10μH
Cin: 4.7μF
Cout: 10μF


Best regard.
Bon Lee.