This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63030EVM-658: The input current range of TPS63030EVM-658

Part Number: TPS63030EVM-658


Hi

My customer purchase TPS63030EVM-658 use Li-ion supply voltage and regulate 3.3V, 0.04A output.

The query is when the Li-ion voltage drop less than 3V the output voltage 3.3V but the current is 350mA, the current is too large for his design, how to solve this issue when Vin< Vout, output current increase?

Thanks

Star 

  • Hi Star,

    What is the customer specification for the application:

    • input voltage range
    • output voltage; 3.3V
    • output current: 40mA?

    If Vin>Vout is the output current 40mA or 350mA during customer test?

    Which changes customer did on the EVM?

    Best regards

    Lubomir