Hello all,
I have a question about PWRHOLD pin high level.
The TPS65910 datasheet shows
Page8 : PWRHOLD pin is connected VRTC or GND.
Page11 : Input voltage rangd of PWRHOLD pin is 1.65 - 5.5V
Page15 : Input high level is 1.35 - VCC7.
SWCA139b schematic check sheet shows
P4 : PWRHOLD pin is connected VRTC or GND
PWRHLD pin is connected to VRTC or GND. Not 5V or GND.
Correct?
Regards.,
Mitsuharu Iwasaki