Hello,
My customer considers a siquence using tps54302's EN.
It's datasheet is written bellow.
(From DEATASHEET ) 7.3.5 Enable and Adjusting Undervoltage Lockout
The EN pin has an internal pullup-current source which allows the user to float the EN pin to enable the device. If
an application requires control of the EN pin, use open-drain or open-collector output logic to interface with the
pin.
(Quention)
Can I use CMOS input for TPS54302's EN controlled.
Regards
Taichi Nakamura