This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS61046: 5Vin to 12V, 200mA out allowable?

Part Number: TPS61046


Tool/software: WEBENCH® Design Tools

I am looking to boost 5Vin to 12Vout at about 150-200mA and was thinking the TPS61046 would be the simplest option and work well, but the WEBENCH designer says it is not compatible. As far as I can tell, the datasheet implies that it should work. Is there something I'm missing?

The load will be an external sensor that will be controlled by a switch on the 12V side.

Caleb