HI, all
In my project, i want to reserve 1.2Wh when the RSOC is report to 0%. We are checking the reserved capacity under different load(20%, 50%, 80% of max power).
What i set for reserve capacity is 120cW. However, only 900mWh is reserved during 80% of max power(RT).
From TRM, this parameter is compensated by discharge rate.
Note, 1.2Wh is reserved during 20% of max power(RT).
load mode = 1 (power)
load select = 3 (average voltage x average current)
BR.
J.C