Other Parts Discussed in Thread: BQSTUDIO, , EV2400
Hello,
I am working with the BQ40z50-R1 to build a BMS for a lithium battery pack. The battery pack has a 3S cell configuration, each cell has a nominal voltage of 3.7V. After receiving the circuit from a third party company that designed the BMS, I can't seem to connect to BQSTUDIO since it doesn't recognize the BMS. When I try connecting the cells to the BQ40z50-R1 EVM it works perfectly, so I'm guessing the problem is either the way the PCB was made or something in the configuration the designers programmed. Also, to communicate I am using the EV2400. Attached find a section of the schematic showing how the SMB pins were connected.
If the connection is ok (I already verified in the PCB it is indeed connected as shown), is there anything in the configuration that could cause a permanent shutdown? Any suggestion on what to do would be appreciated.
Thank you very much,
Luis