Hi Everyone, Im new to this forum so sorry if this is a repeated or obviously question.
I have designed a circuit with this regulator intended to take input from a 9V battery and regulate it to 5V for an attiny microcontroller. I first tried testing just the LM3480 with the battery but it pulled >2.5A when connecting the battery with no load attached to the output. The output voltage swings up and down and sometimes negative.
I have attached two 0.1uF capacitors to the input and output, respectively, as shown in the data sheet. I checked all of my connections for shorts and everything seems to be connected correctly.
Is there something obvious I did wrong or didn't understand from the datasheet about this regulator? I've attached my circuit for the regulator below.
Thank you in advance!