This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/BQ27545-G1: Reset time after DM update of flash gauge

Part Number: BQ27545-G1


Tool/software: Linux

Is there a delay during which a flash (ie non-config-update) gauge resets itself after BlockData and BlockDataChecksum are written?

For the 545, I see "DF block write typically requires a maximum of 72 ms" but I don't see mention of chip reset time.