Other Parts Discussed in Thread: UCC28089,
Hello team.
I would like to have an application to achieve sync_operation with UCC2800 by using UCC28089 SYNC signal.
Now we are examining an attached configuration to do it.
- If you have anything to improve on the attached application or any other recommended configuration, please tell me them.
On UCC2800 datasheet, Fig-19, 1V pulse amplitude as SYNC pulse across 50ohms has been recommened.
- What is the reason why 1V is recommened? and What concerns is there when the pulse with amplitude over 1V is used?
Best regards,
Hidekazu Someno.
UCC28089_UCC2800 Sync_Appl.pdf