Other Parts Discussed in Thread: BQ24253, , TPS61230, TPS61230A
Hello
I'm designing a small battery bank for a product, and I picked the mentioned step up IC.
I designed a PCB to test it along with the bq24253 battery management IC and it works fine.
I tried to stick with the recommended PCB layout for the TPS to avoid issues.
It all was fine until I connected the Moto G Play smartphone to charge it, that is when the issue appeared.
When that particular phone was being charged, the TPS would short the switching inductor to ground as long the phone was being connected.
That would result into a constant DC current of 5A flowing through the inductor and IC, overheating and damaging both components.
At first I did not use the recommended components found in the datasheet so I ordered the exact one specified but the issue persisted.
In no other scenario I managed to replicate the issue, I tried using static DC loads (programmable load), and charging various other phones.
I'm suspecting that the switching mosfet latches up somehow due to some interference caused by the phone, but I'm not sure.
Another thing I noticed is that when charging that specific phone with a regular wall charger, the charger would make an unusual noise.
The issue happens very abruptly so its hard to probe what is going on. Charging the same phone with another step up IC did not cause any issues.
What could be wrong here and is there a way to fix the issue?