Other Parts Discussed in Thread: LM5141, TPS55340
Hi,
Im trying to build the hold up circuit design using TI Boost and Buck converter.The scheme is proposed below.
While testing the module individually everything works fine.When its integrated the Buck converter not responding properly.Buck converter should supply the power to the load when diode turns ON.The diode will turn on only when 10V goes below 9V .
Im validating this solution using TI eval board.I have modified the components based on the Webbench recommended component.
I have changed the L value from 2.5uH to 10uH,Rcomp=14.7K,Ccomp1=3.3nf,Ccomp2=2.7pF.
RFBT=71.5K and RFBB=11K
But not able to succeed it.
Can you pls help me in this.
Thanks-Arumugam
Can you pls help me in this.